Please get in touch with your local Hilti representative, or request a consultation from the Hilti website.
ON!Track Unite is an add-on to ON!Track that can be requested to your local Hilti representative.
Built-for-you integrations are connectors that are built by Hilti or its partners and made available to any customer requesting them. They are ready to be configured and used without any coding required. On the other hand, build-your-onw integrations are coded by ON!Track customers or by their IT vendor and can be customized to fulfill specific customer needs and match with their digital ecosystem.
Yes, visit our built-for-you maketplace to get the whole list of the readily available integration and their details. If the software you use is not among these in the marketplace, or you’d like to customize the integration flows and use cases, you can leverage the API to build a customized integration.
It means that the integration was built and is supported by Hilti.
It means that the integration was built and is supported by an Hilti partner, the contact details are found in the dedicated marketplace’s entry.
There may be some fees required to activate and/or use the integrations listed in the marketplace. The Hilti or partner representative will be able to provide additional details.
In case that the integration used to work but no longer does so, please get in touch with our support team.
Please get in touch with our support team.
It depends on the country where you are calling from, please visit the support page for more details.
Please fill out the form you find on the first page of the help center (form).
Please fill out the form you find on the first page of the help center (form).
Probably there is an issue with the editing workflows in the connector, refer to this tutorial.
They can be requested to your local Hilti representative and they are shown in the “Company Setting” of your ON!Track account.
We recommend to use Postman.
For at least 15 months, more information is found in the API lifecycle page.
Refer to the dedicated section.
Notification will be posted in this developer hub.
No.
Yes, the API connector would have to handle the mapping / conversion logic and further process the data (e.g. from JSON to CSV and upload to a FTP server).
Please have a look at out Release notes log.
For the moment, we only offer one set of API credentials that are sufficient to connect with one external application only. However, we are working on changing that limit and allow more external applications to be connected with ON!Track.